STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1431 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 560 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

How to adapt "LwIP_HTTP_Server_Netconn_RTOS" example from NUCLEO-F429ZI evaluation board to an application with STM32F429VET6 microcontroller?

I am trying to adapt "LwIP_HTTP_Server_Netconn_RTOS" example from NUCLEO-F429ZI to a new project based on STM32F429VET6 microcontroller with STM32CubeIDE, but the connection is not accepted when 'netconn_accept()' function is executed, as I have test...

Ml.1 by Associate
  • 990 Views
  • 0 replies
  • 0 kudos

Example project STM32H747I-DISCO with STM32CubeIDE and STemWIN

Hello, I'm struggling to get an example project running for the STM32H747I-DISCO board within SMT32CubeIDE together with STemWIN. I only want to show simple text and values on the display, updating once a second. I tried to import existing projects...

KR51K by Associate III
  • 837 Views
  • 0 replies
  • 0 kudos

Timer callback function created by RTOS does not working .

I am a biginner of STM32CubeIDE. I made an example which run timer function with STM32cubeIDE. But the timer callback function is not run, Even though osTimerStart() is called in StartDefaultTask() function. What should I change?Thank you in advance...

YDOOY.1 by Associate II
  • 1534 Views
  • 0 replies
  • 0 kudos

Resolved! Warnings Disappear after the second build.

I'm going back over a project trying to clean up all of the warnings.The first time i build the project there are a few hundred warnings. So i clean a few up and build again to make sure i didn't break anything but then all the warnings are gone. Can...

xrstokes by Associate III
  • 2176 Views
  • 2 replies
  • 0 kudos

Set elf file path relative to project

Hello,I have a project structure as follows:Srcbinapp.elftoolsIDEin IDE I have my Stm32CubeIDE and I tried to set the application path to be relative, it get recognized but when launch I got null exception. any clues?

0693W000004IaYpQAK.png 0693W000004IaYuQAK.png
AWahd.1 by Associate II
  • 1394 Views
  • 2 replies
  • 0 kudos

How to configure USB Host and RTOS?

I noticed that STM32CubeIDE 1.4 does not work in the same way as IDE 1.0 with RTOS and USB Host. In IDE 1.0 it is possible to get messages from Degug but in IDE 1.4 not even the messages are displayed.When the uC is started with the pendrive already ...

by Not applicable
  • 1826 Views
  • 4 replies
  • 0 kudos