Fault input for HRTIM is configured as output??
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-04-22 7:57 AM
Hi, I am working with the HRTIM in the STM32G474 Nucleo and trying to configure the fault input to reset the outputs.
When I see in the GPIO config of the HRTIM in the STM32CubeIDE I see that the fault input pin HRTIM_FLT1 is configured as Alternate Function Push Pull and if I use a 220 ohm resistor (to prevent a short circuit) in the HRTIM_FLT1 pin and also measure the input, it still 0V. It seems that the input is... not an input :\
Also in the attached code I see that pTimerCfg.FaultEnable = HRTIM_TIMFAULTENABLE_NONE, and I think it should be HRTIM_TIMFAULTENABLE_FAULT1, it is right?
Also in the registers I can see that FLTxR = 0 and it should be 1:
Bit 0 FLT1EN: Fault 1 enable
0: Fault 1 input ignored
1: Fault 1 input is active and disables HRTIM outputs
What I am doing wrong?
The HRTIM initialization code is attached
- Labels:
-
HRTIM
-
STM32CubeIDE
-
STM32G4 Series