STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1463 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 569 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Why no example code for STM32F0Discovery?

The STM32F0Discovery board comes with accompanying example source code, traditionally. However, now, the relevant download page advises that this is all provided by STM32Cube, but it is not. There is NO example code in the STM32CubeMX / IDE for this ...

Resolved! How to change memory areas in CubeIDE?

If I need to change memory areas in project (for example for Read-only memory I need 0x8080000 start, 0x40000 size), how can I do in in CubeIDE ? (addition) I have found Build analyzer, but the fields are not changeable, only view.

STM32F4 training ?

Hi, I have found 12 videos on Youtube for the STM32CubeIDE - basics but these require the use of a Nucleo-G071RB board.I have an STM32F407VGT6 based Discovery board. Does ST provide any training materials for the STM32F407 line of MCUs utilising the ...

I have a Nucleo-F030R8 and a STM32 Discovery MB1034B which has an STM32F051R8T6 which I am programming from the STM32CubeIDE environment. They don't function the same in Device Manager definitions of capabilities.

Under the Device Manager "Universal Serial Bus devices" \tThe Nucleo board is identified as "ST-Link Debug" whereas the Discovery board is identified as "STM32 STLink" though they show the same driver. Further, the Nucleo creates a "COM" device whic...

RSimp by Associate II
  • 1763 Views
  • 2 replies
  • 0 kudos

stm32cubeide code error

I tried running the first program, but this error occurred. I haven't done any coding, but I don't know why this error occurs.

0693W000004J3LLQA0.png

Can I use preprocessor commands in linker script and how ?

Hey,Is it possible to use preprocessor commands in linker script file (***.ld) and how it can be done if possible. I want to have diffrent memory definitions depending on the macro. I tried this but it's not working:/* Memories definition */ MEMORY {...

JureL by Senior
  • 6778 Views
  • 2 replies
  • 0 kudos

STM32CubeIDE update 1.4.2 cannot be found on 1.4.0

OS: openSUSE LinuxTrying to update from 1.4.0 to 1.4.2 by clicking Help->Check for updatesResult: "No updates found. Configure available software sites to reach more content."STM32CubeIDE Releases is enabled and when I reloaded it, I saw that it does...

VNorr.1 by Associate
  • 2053 Views
  • 3 replies
  • 0 kudos

I have a problem with the STM32CubeIDE, it consumtion a lot of memory ram. In the task manager it open many conhost.exe process (i attach an imagen). Can you know how avoid open many conhost?. (sorry for my english)

I've seen that when I compile the code all the conhost.exe processes are delete but after that, the conhost begin to open automatically like in the attach imagen.

VRodr by Associate II
  • 7388 Views
  • 7 replies
  • 0 kudos