cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE update 1.4.2 cannot be found on 1.4.0

VNorr.1
Associate

OS: openSUSE Linux

Trying to update from 1.4.0 to 1.4.2 by clicking Help->Check for updates

Result: "No updates found. Configure available software sites to reach more content."

STM32CubeIDE Releases is enabled and when I reloaded it, I saw that it does load 1.4.2

I don't use the IDE, I just need the SDK. Is there a place I can download it?

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Markus GIRDLAND
ST Employee

Could you explain further about the use case? You don't use the IDE but you need version 1.4.2? Is it the latest firmware that you are actually in need of?

What I mean is that I don't use the Eclipse based IDE. Make is sufficient for me.

Forget about SDK, what I actually need most is an update for the toolchain inside the following directory:

/opt/st/stm32cubeide_1.4.0/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.7-2018-q2-update.linux64_1.4.0.202007081208

One reason for this is that we have code written using the tools delivered with 1.4.2 which fails to compile with 1.4.0.

The toolchain has not changed between 1.4.x versions. So, the cause should be something else. Which build errors you receive?