cancel
Showing results for 
Search instead for 
Did you mean: 

Wong DMAx->SxCR->CHSEL registers size on STM32F413 (3 bits instead of 4)

nSTAC.1
Associate II

Hello,

I use:

CubeIDE v1.3.0

STM32Cube_FW_F4_V1.25.0

I want to use DMA1->Steam7->Channel8 on STM32F413CHU

During debug, into SFRs window, I found DMAx->SxCR->CHSEL registers size is 3.

Therefore channel 8 is unreachable this way.

However, datasheet RM0430 Rev 8 (p.238/1324) explains CHSEL is a 4 bit length register.

Is it a bug?

Thanks for your help.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Imen Ezzine
ST Employee

Hi nSTAC.1,

To answer your question, the SFRs window view is generated from an .svd file.

So in this case looks like the bug is related to a wrong definition of DMAx->SxCR->CHSEL size into the SVD.

It will help if you can precise the version of the .svd file containing the bug and from our side we will make sure to fix in upcoming release.

Also if you are interested, I can attach a newer version once we fix while waiting to be implemented in next release for CubeIDE.

Thank you for your feedbacks,

-Imen

Imen Ezzine
ST Employee

Hi nSTAC.1,

Just an update, the reported bug is fixed and the new SVD file will be integrated within CubeIDE in their upcoming release.

-Imen