STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1500 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 572 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Hello, I'm new here. I just got a STM32F769IDISCO board. I'm wondering what toolchain should I used.

Let me introduce the situation. I download STM32CubeIDE from st.com, also the STM32Cube MCU package for STM32F7 series which provides many demonstrations.The demonstration's project is created by three toolchains and they are EWARM ,MDK-ARM and SW4ST...

Jinyu Z by Associate II
  • 5361 Views
  • 12 replies
  • 0 kudos

In the process of generating the code from the IOC configuration, STM32CubeIDE also deletes manually added source and include file paths.

In my STM32CubeIDE project, the source code and project file directories are different. The source files are available as linked folder. Therefore, I had made a manual configuration for the source file paths and include file paths. Some paths are rel...

Vvine by Associate II
  • 5435 Views
  • 10 replies
  • 0 kudos

STM32H7 dual core debugging

What is ST's response to this document and the fact that I am witnessing such behaviour (see image) ?? Was there simply an error in this document? I was following the doc only to be frustrated by M4 hitting a brick wall with SIGTRAP, there is mention...

0693W000005Ag79QAC.jpg
LBeau.1 by Associate III
  • 5803 Views
  • 10 replies
  • 0 kudos

stm32H474I cannot debug

I just got a STM32H747I-DISCO board. When I try to debug it and load the code to it by using its internal ST-Link and STM32Cube IDE. It says : "Break at address "0xa05f0000" with no debug information available, or outside of program code." And when t...

GunkutA by Senior
  • 4446 Views
  • 10 replies
  • 1 kudos

STM32cubeide gdb st link flash erase error

helloi use stm32cubeide 1.4.0 and cube programmer 2.5.0 i want to st link gdb server​https://community.st.com/s/question/0D50X0000BD4BDRSQ3/error-failed-to-erase-memory​The same symptom appears even if option byte is set and flash is deleted.​The a...

Ykim.4 by Associate
  • 782 Views
  • 0 replies
  • 0 kudos