cancel
Showing results for 
Search instead for 
Did you mean: 

STM32cubeide gdb st link flash erase error

Ykim.4
Associate

hello

i use stm32cubeide 1.4.0 and cube programmer 2.5.0

i want to st link gdb server

https://community.st.com/s/question/0D50X0000BD4BDRSQ3/error-failed-to-erase-memory

The same symptom appears even if option byte is set and flash is deleted.

​The above and symptoms are the same.

I know the solution. About this problem.

The solution was I copied the stld file inside the stlink folder and the problem went away.

Looks like a patch is needed from ST.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0