STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1527 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 580 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! How to configure STM32CubeIDE to use J-link in tunnel mode

I am trying to configure STM32CubeIDE to use J-link in tunnel mode. I know how to do it outside the CubeIDE. It requires the invocation of J-link GDB server with the additional -select command line parameter. And I don't know how to add this paramete...

MirKoz by Associate III
  • 3469 Views
  • 3 replies
  • 0 kudos

What exactly starts the clk during spi communications?

According to section 28.9.1 (of RM0091), the spi communications are enabled when register 6 is active (SPE set to 1). According to the rm0091 guide, once the spi communications are active, and register 14 is set to 0 (receive only mode) then the c...

Iviti.1 by Associate III
  • 5289 Views
  • 12 replies
  • 0 kudos

Slightly overclocking STM32G070 without external oscillator

It runs at 64MHz, and I need it running at 65 MHz. I've managed to create 65 MHz clock in PLL using multipliers/dividers in STM32 Cube IDE, but I'm not able to test it before I order the PCB-s, which I'm not intending to do before I confirm this woul...

Slina by Associate III
  • 3143 Views
  • 7 replies
  • 0 kudos

Latest STM32CUBE IDE problems. Malloc() failure.

I upgraded to STM32CUBE IDE v1.5 few days ago, then strange problems began to appear.Suddenly, code that previously worked on v1.3, doesn't. No major changes.The program uses a some dynamic memory allocation, so to debug the free memory, I use this r...

How to program final 'release version' of code?

I've been programming my chips via the debug mode in STM32cubeIDE, but the code doesn't seem to run properly when the debugger isn't connected. What is the correct way to program a 'final release' version of my code, that will run independently every...

deep_rune by Associate III
  • 3221 Views
  • 9 replies
  • 0 kudos