STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1415 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 558 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

En el Stm32cubeide versión 1.3 existe alguna forma de crear algún proyecto escrito netamente en lenguaje ASM; uso la placa Discovery st.m32f429izt

En el Stm32cubeide versión 1.3 existe alguna forma de crear y escribir algún proyecto netamente en lenguaje ASM; uso la placa Discovery st.m32f429izt; lo que busco es un compilador netamente en ASM que trabaje en el CUBEIDE.Gracias.

LZamb.3 by Associate II
  • 1967 Views
  • 3 replies
  • 0 kudos

Resolved! Finding the function beeing interrupted

Hello,I used to work with IAR.In IAR call stack, if ever you break into an ISR, the call stack shows you where you were in the "main" code just before the ISR fired.Now, with STM32Cube MX, the call stack only shows the call stack since the root ISR ...

Kuikui by Associate III
  • 3104 Views
  • 4 replies
  • 1 kudos

I want to make a USB to CAN Inteface for that I recently bought a USB-CAN Transceiver(Auvidea 70200 - contains STM32F042C6U). I tried to do some CAN testing using STM32CubeIDE Version: 1.4.0.

When I built a sample code and tried to do the Debugging using STM32CubeIDE it was showing that "NO ST LINK detected! Please connect ST LINK and start the debug session.".This Transceiver contains 2 channels of CAN output and one side contains USB 2....

RahulR by Associate II
  • 831 Views
  • 0 replies
  • 0 kudos

1) Debug does nothing (both menu and icon). No messages, no warnings, no logs, nothing. Yet it works at home. 2) In project generate code advanced settings, turned off MX_BlueNRG update options, yet it still overwrites all my changes in modifying service

Originally, it seemed to work okay. Now I can't get it to work at all after many days of trying, and in addition, whenever I write code, my code keeps getting over-written and my files deleted. I have installed openocd, but can't get the ide to downl...

Resolved! hi2c2 in an external .c

Hello to all.I'm coding an I2C comunication and the IDE (1.4.0) create the Private variable I2C_HandleTypeDef hi2c2; and then the function MX_I2C2_Init. Everithing ok.I'm using an external .c file to handle the I2C communication and how can I access ...

MSole.1 by Associate
  • 2045 Views
  • 1 replies
  • 0 kudos

Resolved! STM32CubeIDE 1.5.0 crash issue

Hi,I cannot import existing project into Workspace. Here's the error log when I try to select a root directory: eclipse.buildId=Version 1.5.0 java.version=1.8.0_272 java.vendor=AdoptOpenJDK BootLoader constants: OS=linux, ARCH=x86_64, WS=gtk, NL=en_...

0693W000005CGxXQAW.png
Gaston by Senior
  • 2120 Views
  • 6 replies
  • 0 kudos