STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1429 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 559 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Custom download location to avoid using SSD drive

I am using STM32CubeIDE. It frequently downloads large files from internet (e.g.; device specific file when you start a new project, updates, etc).The problem is, the files are downloaded to my C drive which is SSD. The download location is "C:\Users...

EKarg.1 by Associate
  • 860 Views
  • 1 replies
  • 0 kudos

Importing project issue for EVAL board

I am trying to import (STSW-SPIN3202-V1.0.0 ) to cube IDE. I get the following errors. Seem to be related to the linker config file. The paths are not correct. How do i fix this issue ? I used the "Import" from existing project and file import option...

0693W000006HUbyQAG.jpg
PKAci.1 by Associate II
  • 634 Views
  • 0 replies
  • 0 kudos

Resolved! Debugger will step OK but loses connection

Issues:target MCU programs correctly.debug aborts on resume or run, then target runs by itself.single-stepping works, but if breakpoints are set then on resuming or running then debugger never stops at the breakpoint(s).Debugger connection lost.Shutt...

EAppe.1 by Associate II
  • 2145 Views
  • 2 replies
  • 0 kudos