User Activity

Hi all,SBSFU ported to many custom boards and in projects, and is working as expected. But in a project with Touchgfx throwing error "error was: Firmware signature check failure." on Installing update FW from download area.As it is working for other ...
Hi there ...Is there any document explain the STUSB4710 register map (in stusb4710.pdf)? I have already STUSB47xx_register_map_public.pdf, but nothing detailed!I'll appreciate for any help.With regardsJitu
Hi, I have successfully implemented a complete graphic to display some system related parameter on a monochrome OLED Display with display driver SSD1322, which is a horizontal drawing pixel, however porting the same code to a monochrome OLED Display...
Intergrated USB in SBSFU for FW update, and adapting it to work with YMODEM protocol. Only half of the package is downlaoding to microcontroller. Getting error. I will highly appreciate for any help. = [SBOOT] STATE: HANDLE CRITICAL FAILURE= [EXCPT]...
Under SBSFU, I am able to run my custom application, and everything run fine. But changing the SFU defualt UART.with USB throughing error "USB Device not recognize!!!", I debug through SBSFU code, and USB stack(CDC and Devi ce only Configuration) in...
Kudos from