STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1541 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 586 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Read multiple ADC channels using DMA not working.

Hi, I am trying to read multiple ADC channels using DMA method. I am not able to read values. I am not sure what wrong i am doing. /* ADC1 init function */ void MX_ADC1_Init(void) { ADC_ChannelConfTypeDef sConfig = {0};   /** Common config */ ...

RBV by Associate II
  • 4799 Views
  • 10 replies
  • 0 kudos

How I can change glodal encoding?

Hello,I have changed Preferences->General->Workspace->Text file encoding to Default (windows-1251).After clicking 'Apply and Close' IDE striongly restores this property to UTF-8.I have to use windows-1251 encoding in my project.Nevertheless I see 'À�...

KMiha.1 by Associate
  • 4373 Views
  • 3 replies
  • 0 kudos

Resolved! Can't use different RAM Section

Hello,I'm working with STM32H7 and STM32 Cube IDE,I add this in linker script :/* Memories definition */ MEMORY { DTCMRAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K ITCMRAM (xrw) : ORIGIN = 0x00000000, LENGTH = 64K RAM_D1 (xr...

Debugging hardfault

Hello, I need suggestion in debugging hardfault. I got stack as below, I am kind of unsure how to debug it. CFSR value is 0x00020000 means its INVSTATE.

0693W000007AuZ0QAK.png

avoid flash erasing when debugging

Hello,My simple application should read some configuration which I put by CubeProgrammer from 0x0800C800, I want to debug the application but seems the debugger erases the flash at all. Could you tell me please how to prevent full internal flash eras...

YGU.1 by Associate II
  • 1702 Views
  • 2 replies
  • 0 kudos