cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE Debug Options

EGonc.1
Associate II

I'm using a STM32F401RE and developing on STM32CubeIDE.

Since I have a Bootloader on address 0x08000000 and I had to move the Application to 0x0800C000 by changer the linker file:

MEMORY

{

 RAM  (xrw)  : ORIGIN = 0x20000000,  LENGTH = 96K

/* FLASH  (rx)  : ORIGIN = 0x08000000,  LENGTH = 208K */

 FLASH  (rx)  : ORIGIN = 0x0800C000,  LENGTH = 208K 

}

Now when I try to run the Application under STM32CubeIDE it crashes which seems obvious since the Debugger needs the VTOR properly initialised.

I have commented the line in SystemInit() that initialises the VTOR.

void SystemInit(void)

{

 /* FPU settings ------------------------------------------------------------*/

 #if (__FPU_PRESENT == 1) && (__FPU_USED == 1)

  SCB->CPACR |= ((3UL << 10*2)|(3UL << 11*2)); /* set CP10 and CP11 Full Access */

 #endif

#if defined (DATA_IN_ExtSRAM) || defined (DATA_IN_ExtSDRAM)

 SystemInit_ExtMemCtl(); 

#endif /* DATA_IN_ExtSRAM || DATA_IN_ExtSDRAM */

 /* Configure the Vector Table location add offset address ------------------*/

#ifdef VECT_TAB_SRAM

 SCB->VTOR = SRAM_BASE | VECT_TAB_OFFSET; /* Vector Table Relocation in Internal SRAM */

#else

// SCB->VTOR = FLASH_BASE | VECT_TAB_OFFSET; /* Vector Table Relocation in Internal FLASH */

#endif

}

I hoped that in Debug Configurations | Startup | Specify Vector Table (hex) I could just write 0x0800C000 and the VTOR would be initialised by the Debugger...

But doesn't seem to be the case! After download and with a breakpoint in the Reset_Handler I can see the VTOR as 0.

Does anyone know how to change the address of the Application to a different than 0x08000000 and still being able to Debug.

thanks

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0