STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1579 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 598 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Instabilities are occurring in Version 1.6.1

I'm using version 1.6.1 in linux, and there are several problems, for example, the main.c file opens but I can't use Delete or BackSpace keys, other times I can't edit the properties of the Device Configuration Tool. It has also occurred that the Dev...

by Not applicable
  • 1026 Views
  • 1 replies
  • 0 kudos

STM32CubeIDE 1.6.1 Update Fails on WIndows 7

I have gotten update notices for STM32CubeIDE 1.6.1 for a couple weeks now. But every time I try to update it fails. I did try deleting the cache directory "STM32CubeIDE\STM32CubeIDE\p2\org.eclipse.equinox.p2.repository\cache" but that did not work...

Resolved! No binary or hex file output

Hello,I've a strange problem with CubeIDE 1.6.0, there's no binary or hex file output even if the corresponding outputs are activated under MCU post build outputs. Any ideas what might be the issue there?Regards

RAltm by Senior
  • 12023 Views
  • 20 replies
  • 1 kudos

After upgrading to STM32CubeIDE 1.6.1 the .cproject file gets messed up with spaces instead of tabs and extra blank lines (spaces + tabs) between each normal line. This messes up any source control system.

prior 1.6.1:<?xml version="1.0" encoding="UTF-8" standalone="no"?> <?fileVersion 4.0.0?><cproject storage_type_id="org.eclipse.cdt.core.XmlProjectDescriptionStorage"> \t <storageModule moduleId="org.eclipse.cdt.core.settings"> \t \t <cconfiguration i...

Martin_S by Associate II
  • 1327 Views
  • 1 replies
  • 1 kudos

LWIP HTTP Server. Packets retransmittion.

Hello, dear colleagues!I'm trying to build http server based on LWIP on Nucleo F429 board. An example from Cube repository works fine, also with my custom http data and paths, which I have included in example project. But, another CubeIDE generated p...

0693W000008xyvvQAA.png 0693W000008xyzdQAA.png

Resolved! Why doesn't compiler find defintion of the function (it says undefined reference to `osSemaphoreWait') on the link step ?

I have #include "cmsis_os.h" statement in my .c file. Also Ctrl+click works in CubeIDE to get to the correct file that includes definition of the function (cmsis_os.h) and also reports correct directory (CMSIS_RTOS_V2)...Really weird behaviour, I'd ...

bully by Senior
  • 3345 Views
  • 1 replies
  • 2 kudos

How to disable error popup window.

Hello!I'm using STM32CubeIDE 1.6.1. This question is not specific to 1.6.1, the problem (or feature???) existed before.When debugging (build and debug, or press the green bug), if there are errors, the IDE asks me if I want to run (proceed with launc...

PG.1 by Associate III
  • 2162 Views
  • 2 replies
  • 0 kudos

STM32CUBEIDE DEBUG PROBLEM

HelloMy debugger is shutting down after downloading code into chip I can connect STLINK UTILITY and uploading code hex files properlySTMicroelectronics ST-LINK GDB server. Version 5.8.0 Copyright (c) 2020, STMicroelectronics. All rights reserved.   S...

Proteus by Associate II
  • 1216 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.