Hello,I'm working on a low-power application using the STM32L073 microcontroller and aiming to achieve a current consumption of around 3.5 µA in Stop mode. Here are the steps I've followed so far:Power Connections: I'm powering the microcontroller di...
Hello,I was trying to understand the leakage in my STM32L073 based board. After programming with this code for 3 different boards I am now unable to connect to board both using the programmer and IDE. I have tried BOOT0 and nRST combo to connect but ...
Hello Everyone,
I am trying to build the project from the pack "STM32CubeFunctionPack_LTE1_V1.1.0". I am using CubeIDE 1.12.0. Kindly help me build the project, I am new to STM32 CubeIDE. Thanks and regards.
Hello,I am using FreeRTOS for my prject using STM32F746 with STM32IDE. Is there a way I can use a trace tool? I have come across Segger System View, is it compatible with STM32IDE?Regards,Prudhvi Sagar
Hello,I am new to STM32 family and have been using STM32Cube IDE for the past 2 months. I am working on FreeRTOS based project and am looking to use SEGGER's Systemview. I am trying to follow the steps given but am unable to patch FreeRTOS folder and...
I have taken OFF the SBs going to ST-LINK and now observed that the power consumption is 0.44 u amps. NRST is the culprit is what I see but this current feels very low is it correct? The code I have used is this /**
********************************...
Hello Andrew,I have looked into the schematics and observed USART, MCO, NRST, SWO pins connected over solder bridges to the ST Link where CN2 separates out the required programming pins. So I take off the SBs then you think I will be able to achieve ...
Hello Kaouthar,The changes you mentioned has resolved the issues for 1.5.1 but not 13.1. I have attached an image for reference. Now I can get started with the project. Thanks and regards.
Hello Kaouthar,I am still getting the issue. I have attached the screenshot. I have exactly done what you have suggested. Kindly let me know what can be done I will do it as you suggest. Thanks and regards.