STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1427 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 559 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Pointers and HAL libs => HardFault?

I'm having a problem that I don't understand why it happens.I am using STM32CUBEIDE (updated).Each time the code below runs, the PC jumps to "HardFault_Handler". But I can't understand what the problem is ...uint8_t buff_cfg[10] = { 0 };   bu...

Is there a way to configure the internal memory (SRAM, Flash..) of STM32F769 as frame buffer for LTDC by using STM32CubeIDE?

I am now working on a STM32F769 based board without external memory to communicate with a LCD via RGB interface. I want to use STemWin stack libraty but I can not enable it because some misunderstanding, the GRAPHICS in the Middleware section is stil...

NHuy.12 by Associate
  • 1053 Views
  • 0 replies
  • 0 kudos

Error loading during project generation

Error loading during project generation, access to the network is allowed in the firewall, the folder with repositories is empty, I can’t download any repository through the program. I just installed the development environment. I don’t want to manua...

RVolo by Associate
  • 1185 Views
  • 1 replies
  • 0 kudos

stlink v2 no device

At first, I downloaded elf using stlink v2 and run firmware. and then rebuild source. After that I tried to run debug button. But I encountered no device message.

Clee.4 by Associate II
  • 933 Views
  • 1 replies
  • 0 kudos

STM32CubeIDE does not support external tools

In TrueStudio, it was able to bind an external tool to a breakpoint. I can still select the "External tool action" in the breakpoint properties dialog, but I can't add an external tool in the "External Tools Configuration" dialog. Will this feature b...

SBusc by Associate
  • 1506 Views
  • 1 replies
  • 1 kudos