STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1548 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 587 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Can't build a project after importing it

Here's the scenario:I have clean workspace. I have two projects on disk I want to import into the workspace. I store them on my Google Drive locally sync'd to my computer (Windows 10).I import one of the projects and try to build it. I can't beca...

Resolved! [SOLVED] Weird behavior debugging STM32H753

Dear experts,I hit a strange problem when debugging in CubeIDE code with a bootloader on Nucleo STM32H753.The bootloader sits in sector 14. The boot address of STM32H7 is redirected there via the option bytes. The main code starts at sector 0 (a.k.a....

Pavel A. by Super User
  • 1520 Views
  • 2 replies
  • 0 kudos

STM32CubeIDE crash on Linux.

I've installed the STM32CubeIDE on MX Linux in both versions (Generic and Debian Linux). Every installation crashes first after the search for targets. After some tries the software found successful the parts. Then I have crashes after the normal sta...

HHoop by Associate
  • 1635 Views
  • 2 replies
  • 0 kudos

CubeIDE / GCC Flash code placement... How to split the program into more than one flash sector and leave a 16K sector empty in-between ? STM32F446

Where might I find the information to do something like this ? Need to make good use of flash space and would like to keep one of the 16K sectors for updatable calibration data.I would think this would be one solely in the linker script but evidentl...

constant data structure can't be watched

I have a project which use STM32H743ZI, and i have a data structure#define APP_MODULE_MAJOR (INT8U)0x01 /*!< Major version of the APP module */ #define APP_MODULE_MINOR (INT8U)0x01 /*!< Minor version of the APP module */ ...

0693W00000BdfiQQAR.png
MFawzy by Associate III
  • 1672 Views
  • 3 replies
  • 0 kudos

Resolved! How to enable Segger debugger in STM32CubeIDE v1.1.0

I created STM IDE project from the scratch. I'm using STM32H742Zi Nucleo board. When I configure the debugger I have only two options , all to them are ST-LINK debugger. See attached picture.This features worked flawlessly in Atollic True Studio.The ...

MMagl by Associate III
  • 3815 Views
  • 5 replies
  • 0 kudos

CubeIDE debugger vs Atollic, how to make a startup script?

Apologize if this was already asked, I cannot find answers here.In the Atollic debugger config there's a Startup script tab.Default script looks like this:# Set flash parallelism mode to 32, 16, or 8 bit when using STM32 F2/F4 microcontrollers # Unco...

Pavel A. by Super User
  • 1672 Views
  • 2 replies
  • 0 kudos

Resolved! STM32CubeIDE drives me crazy at the moment...

Hello,Right now the IDE is driving me crazy: I've written an include in my project, made requred/mandatory entry in project settings (see the attachement), and get the error message "No such file or directory" when I compile the project.I've checked ...