User Activity

Somehow my STM32CubeIde does not allow to put breakpoint at any project see attached picture.I've read that this issue can be caused by too many projects on workspecae - I reduced the number of worspace procect but still does not workI thinks that I ...
I have upgarded several old NUCLEO boards without any problem. All boards ware equipped with ST-LINK-V2 debugger I've tried to upgrade two new Nucleo boards board equiped wit ST-LINK-V3 .Result : Both returns error during upgrade. See attached scre...
I created STM IDE project from the scratch. I'm using STM32H742Zi Nucleo board. When I configure the debugger I have only two options , all to them are ST-LINK debugger. See attached picture.This features worked flawlessly in Atollic True Studio.The ...
Rev V system boot loader FDCANSTM introduces boot via FDCAN1 with chip revision V.The system boot loader version ischanged form V13.3 to V9.0. I’ve tried to figure out how does it work. Here are my findings-     AN2606 rev 38 is updated. It describes...
According to following white paper, some STM32 MCUs has security issues.https://www.usenix.org/system/files/conference/woot17/woot17-paper-obermaier.pdfThe question is Which STM32 components are affected?We are considering to use STM32H750vb and STM3...
Kudos from