STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1328 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 529 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32CubeCLT download option for macOS AArch64

On the download page for the STM32CubeCLT software, there is only a single download option available for macOS (STM32CubeCLT-Mac), which downloads the x86_64 version of the software.Are there plans to add a download option for AArch64 macOS?

Resolved! STM32 cube IDE with code generator and CMake

Hello Experts,I am looking for a solution in which we can create STM32 project with .ioc file and generate the code but cmake as build tool instead of make.I know we have couple of options while creating new project as follows:We can either create ST...

PatelHarsh_0-1760651709094.png

Resolved! STM32Cube IDE 1.15.0 issue

After updating Cube IDE to version 1.15.0 the memory details & memory regions map in the build analyzer are not showing any informations beside the linker script file name in all my projects start to be bold!!!

MSale.1 by Senior
  • 4189 Views
  • 4 replies
  • 1 kudos

Account login issues caused by STM32CubeIDE 1.19.0

 When I try to log in to my account, the software prompts "Connection lost"After I rolled back the version to 1.17, this issue disappeared. Many users in the China region have encountered this problem, and it’s unclear if it exists elsewhere.

ZnMnCr_1-1760846758224.png
ZnMnCr by Associate II
  • 441 Views
  • 1 replies
  • 0 kudos

Failed to execute MI command

I am trying to debug my hardware for the first time. I was working in TrueStudio 9.3.0 as I had started this project in it before STM32CubeIDE came out. When I started to try to debug my program to day I got an error. OK, maybe I should try STM32C...

Resolved! Can't Run or Debug from CubeIDE

HiI don't know what happens, I just restarted my laptop, then it does not run or debug from CubeIDE. Before I retarted the laptop, I was debugging.When I click to Run or Debug, there is nothing appearing in the console window.  I closed the IDE twice...

Chao by Senior II
  • 3377 Views
  • 21 replies
  • 3 kudos

Resolved! STM32H757 SWO Debug Error

Hello,I am experiencing the same issues as these individuals : https://community.st.com/t5/stm32-mcus-products/stm32h757-swo-debug-error/m-p/738531#M265220When I launch my debug with SWO enabled, I encounter errors upon launch, and if the errors are ...

MA4 by Senior
  • 534 Views
  • 1 replies
  • 0 kudos