STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1427 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 559 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Failed to list external Loader

I try to add external loader to C:\ST\STM32CubeIDE_1.8.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.0.100.202110141430\tools\bin\ExternalLoaderIn debug configuration, check ExternalLodaer and than press Scan.Th...

ALomb.1 by Associate III
  • 8665 Views
  • 20 replies
  • 0 kudos
ltan.11 by Associate
  • 1725 Views
  • 1 replies
  • 0 kudos

Clicking on Search result opens the file in new Editor

Hi,This problem is observed in v1.9.0 as well as in earlier versions. If one clicks on any search result to open the respective line then the file is opened in a new Editor, despite the fact that the same file is already opened in another editor wind...

davhak by Associate II
  • 1476 Views
  • 4 replies
  • 0 kudos

Resolved! STM32Cube IDE app fails to run on latest macOS Monterey beta

I'm running the latest (less than one week old) macOS Monterey developer beta 12.4 (build 21F5063e) on a MacBook Pro 10,1 and downloaded the file en.st-stm32cubeide_1.9.0_12015_20220302_0855_x86_64.dmg_v1.9.0.zip, decompressed and installed the app. ...

0693W00000LzXVXQA3.png
mikew67 by Associate II
  • 2005 Views
  • 2 replies
  • 0 kudos

STM32CubeIDE 1.9.0 Question: User generated .c&.h files don't have the same functionality as the auto generated files like main.c.

I can add my own .ch files to a project and build and see the proper functionality on the MCU with no problems. However, the user generated src modules are not colorized, or system calls are not "Auto Complete" enabled like main.c module is. More imp...

FAssa.1 by Associate
  • 1108 Views
  • 3 replies
  • 0 kudos

Why SWD stopped working after re-programming?

I have an STM32G030 board that I was debugging, and all was going well. Then I started getting an 'unable to connect' message while debugging. Reading some of the forum, the issue appears to be that I checked "Set all free pins as analog (to optimize...

RLour.1 by Associate II
  • 5000 Views
  • 6 replies
  • 1 kudos

stm32 rx and tx interrupts interfere with each other

Hello,I am using STM32H743 Nucleo-144I have an RX EXTI interrupt which reads multiple SPI messages (a very busy channel)also, a TX interrupt which reads UDP messages dose small calculation and sends the new messages with SPI channel (pretty busy too)...

Mz.1 by Associate III
  • 2878 Views
  • 4 replies
  • 0 kudos