STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1550 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 588 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Indexer problem in STM32CUDEIDE 1.8 and 1.9

Hello dear friends,I have installed STM32CUBEIDE v1.7, v1.8 and v1.9. Since V1.8 the indexer can't find variables and functions in cube-generated files and throw this type of message."Could not find symbol 'blah blah' in index".This issue is really a...

I am working with CubeIDE 1.7.0 . I was to move my project on latest 1.9.0 version, but this version of CubeIDE is give me 500 errors . Do you know where I can download CubeIDE 1.3.1 again ?

stm32 cubeide 1.9.0 version gcc 10 compiler give me error in structures files but in 1.7.0 version of software gcc 9 all ok with structure.maximum error cover with the help of extern before variables and function but only problem in structure defini...

SKapa.1 by Associate II
  • 2842 Views
  • 5 replies
  • 0 kudos

as we discussion we move stmcubeide32 1.7.0 version to stmcubeide32 1.7.0 we are solve the multiple error resolve with the help of "extern" but some error reaming regarding structure declaration give some error in gcc 10 not resolve

1.sturcture declaration we have facing some errors in the GCC 10 in terms of the variables and function we use "extern: solve the error 2.But in terms of structure how we resolve the errors please look the issue and give me some solutions .

SKapa.1 by Associate II
  • 2242 Views
  • 3 replies
  • 0 kudos

[BUG FOUND] Printf/Sprintf for float point variables not working.

I found a quote that this problem had been fixed in an earlier version, but the problem is reoccurring. Using STM32CubeIDE Version. 1.2.1 Build: 5190_20200115_1224 (UTC)This problem is fixed in STM32CubeIDE ver.1.0.2.Still need to add the flag:Workar...

0690X00000ByaxXQAR.jpg
by Not applicable
  • 1220 Views
  • 2 replies
  • 1 kudos

Resolved! STM32CubeIDE: why when I specify Core/Inc path as include path, IDE shows warning about missing CM4/Debug/Core/Inc?

I try to specify relative paths without a lot of ../../.. spaghetti, but every time I shoot into the correct directory, I get an error like a /Debug/ was added to my path?I moved all my code files, now I want to make include paths right, but it's eit...

HTD by Senior III
  • 9179 Views
  • 3 replies
  • 1 kudos