STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1553 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 588 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32H725 SD Card errors after debug suspend

While debugging, program execution after (or during) sd card initialization causes the SDMMC module to return errors while executing commands for subsequent calls.STM32CubeIDE v1.10.0, Build 12671_20220627_1643Debugging with STLINK-V3MINIEUsing the a...

JOlso.1 by Associate II
  • 1809 Views
  • 2 replies
  • 0 kudos

Dual core debug

I'm trying to get up to speed on dual core debug on the STM32H745 Disco, using STM32CubeIDE. I've followed a couple of instructional videos that show how to do this.https://youtu.be/k3mXhPZSaswhttps://youtu.be/jI1k6p-fduEI've got both cores blinking ...

Resolved! My project is building successfull but cannot upload it to STM32Discovery board and the stm32cube ide is showing libncurses related error on Manjaro Linux.

Below error is throwing in Manjaro Linux when I try to upload the program to the board. The project is building successful. Installed libncurses from AUR as well as the offiicial repository, but no use.

0693W00000QKn7oQAD.png

CubeIDE: debug multiple instances of a project?

either to debug multiple instances of the same project; eg, two BLE peripheralsor to debug multiple projects; eg, a BLE Central and a BLE peripheral.In the latter case, I guess you could put each one in a separate Workspace - but that doesn't help in...

STM32CubeIDE Multiple STlink Debug of same Project

We have a system of many interconnected STM32 boards of various types.Today I need to debug two identical boards of same type.I can step code in two different STM32 projects by starting two IDEs,but ...When I start multiple IDEs and try to do debug w...

Paul1 by Lead
  • 3386 Views
  • 3 replies
  • 0 kudos