STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1553 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 588 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Need a working project with FreeRTOS and FATfs with CubeIDE Version: 1.10.0 and STM32CubeF4 Firmware Package V1.27.0

Hi community, Please provide me with a working example with CubeIDE Version: 1.10.0 and STM32CubeF4 Firmware Package V1.27.0 which contains both FreeRTOS and FATfs.The DMA handling seems buggy after several releases and none of the fixes mentioned in...

NSeba by Associate III
  • 1921 Views
  • 3 replies
  • 0 kudos

[resolved] Rename/Checkout STM32 Project to different folder

Sometimes I end up working on multiple branches of a project (ain't life fun!).With STM32CubeIDE it seems if I rename the project folder Project Project_Main Project_BranchXThen the Sources paths defined in the project are broken/lost, and any exclud...

Paul1 by Lead
  • 3867 Views
  • 5 replies
  • 0 kudos

Resolved! How to programming using JTAG

Hello,I am using the STM32CUBEIDE , I am working on STM32H745 series , I have to programme the device using JTAG .How I can done that which application I have to use for progrraming what setup I have to done in stm32cubeide ? Can u please help me

MDeva.1 by Associate II
  • 11612 Views
  • 3 replies
  • 0 kudos