STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1554 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 588 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Unable to enter debug mode

I'm new to ST32 series, I bought a NUCLEO-L476RG and a B-L475E-IOT01A to get started. When I plug in either of these boards, it installs itself as a ST-Dongle and ST-Virtual COM port. When I execute my code it flashes the board, it starts my code but...

Jvan.19 by Associate
  • 6582 Views
  • 8 replies
  • 0 kudos

stm32cube ide build analyzer not working ?

I can't seem to get the build analyzer to show mamory usage in the "memory regions" ?Sometimes it shows, but usually not. What am I doing wrong ? Or what shall I do to get it show the memory usage always ?

MAalt.1 by Associate
  • 8148 Views
  • 2 replies
  • 4 kudos

Resolved! WHAT IS THE static HAL_StatusTypeDef name_funtion()?

I am using an example that i want use in my keil Project. the example is in stm32cubeide with HAL library, i am working in keil with standard peripheral. i want use.I want to change the statement of this function using standard peripheral, I know sta...

jdo by Associate II
  • 2352 Views
  • 4 replies
  • 0 kudos

Cannot debug using RTOS Kernel Awareness

Having an issue trying to view multiple thread contexts with CubeIDE RTOS kernel awareness. The debugger keeps disconnecting when RTOS kernel awareness is enabledNormal debugging using GDB server is function correctly.Upon enabling RTOS Proxy, after ...

0693W00000SumBLQAZ.png
EWill.4 by Associate
  • 2326 Views
  • 0 replies
  • 1 kudos

Resolved! How to update Includes directory

Hello everyone,I have a question about how to update Includes folder in a downloaded example from STM32 CubeMX.Currently, I am working with LoRaWAN_End_Node example downloaded from STM32 CubeMX for the board Nucleo-WL55JC1. Based on that example, I w...

0693W00000SuKQ3QAN.jpg
HNguy.25 by Associate III
  • 2240 Views
  • 3 replies
  • 0 kudos

Failed to execute MI command: -data-disassemble -s 484 -e 760 -- 3 Error message from debugger back end: Cannot access memory at address 0x10000

This Error shows up on various Places in the Memory. I can access the Memory through the Memory Browser, but unfortunately there is no Disassembly Interpretation like in the Disassembly Window. This Errors occurs mainly on SRAM Memory, not in Flash. ...

0693W00000Suj1xQAB.png

lost link/path to gcc after uninstall of IDE and reinstall

When I run my program I get an error:##########16:23:19 **** Incremental Build of configuration Debug for project LoRaWAN_End_Node ****make all 'Building file: ../Utilities/trace/adv_trace/stm32_adv_trace.c''Invoking: Cross GCC Compiler'gcc -O0 -g3 -...