STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1415 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 558 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Hello Everyone, I'm trying to run the sample code given to me by the provider of our board and I'm having a problem when I try to build the project.

This is the sample error that pops up. How can I fix this? I'm very new to this so I'm not very familiar with this error. Hope that someone could help me with this. Tell me what else I need to provide so you can help me better./Applications/STM32Cube...

NPine.1 by Associate
  • 2730 Views
  • 3 replies
  • 0 kudos

Resolved! CubeIDE how to set offset for program?

I am making a DFU for stm32f4-discovery board.My DFU is using a project generated by STM32CubeMX V1.0. And It worked well with the program generated by the STM32CubeMX V1.0But when I worked with a project generated by STM32CubeIDE, I cannot make the ...

binhla by Associate II
  • 5359 Views
  • 4 replies
  • 1 kudos

stm32f745vet does not flash through STM32CubeIDE

After STM32 ST-LINK Utility, everything works fine with such settings, I can flash the hex file, the firmware works.But if I try to enter debugging through STM32CubeIDE 1.0.0, then this error always appears:Error in final launch sequence:   Error in ...

0690X00000ArwBwQAJ.png 0690X00000ArwC1QAJ.png

STM32F429I example projects

I want to start programming the STM32F429I by studying some example programs provided by ST or some users.Online I found few tutorials and someone recommended using the examples in: "STM32Cube_FW_F4_V1.0\Projects\". I tried to open a few examples on ...

luke514 by Senior
  • 8456 Views
  • 7 replies
  • 0 kudos