STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1554 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 588 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! __UNALIGNED_UINT32_READ causes Unaligned Hardfault [solved]

I have trouble with sporadic Hardfaults and I tracked it down to some unaligned access in the USB routines. Although the code uses the macro __UNALIGNED_UINT32_READ, the STM32 will still causes the Hardfault for unaligned addresses. So I looked at th...

SFahr by Associate III
  • 8369 Views
  • 7 replies
  • 1 kudos

Issue on Semihosting on CUBE IDE

Salutations for all.I programmed my CUBE IDE on Debug Mode by the recipe-> https://community.st.com/s/article/how-to-use-semihosting-with-stm32cubeide-and-stm32. It Works.But when I STOP the running program on CUBE IDE the TARGET STOP the program eit...

JSILV.2 by Senior
  • 1830 Views
  • 3 replies
  • 0 kudos

STM32CubeIDE 1.10.1 Does'nt open

Hello , am writing on this forum because i got a problem , and was wondering if anyone could help me . Ive installed STM32CubeIDE 1.10.1 on my pc (windows 10) but am unable to open it for some reason , ive tried looking on youtube ''stm32cubeide dose...

AGrom.3 by Associate
  • 917 Views
  • 1 replies
  • 0 kudos

STM32CubeIDE program flow, Arrow->

I understand, that, when the arrow symbol appears in front of a source line, that means, that the program flow has stopped at that point. But tin fact he case is, that the program is running. Only when I click pause, the arrow jumps to the "while(1)"...

(Solved) My arm_gcc_link script (32F407VGT6U) is not passing the correct fnVector table address. With the script below the MCU is not resetting to the correct location. The fnVector table is at rom address, 0x08010000, any guidance would be appreciated.

OUTPUT_FORMAT ("elf32-littlearm", "elf32-bigarm", "elf32-littlearm")   /* Internal Memory Map*/   MEMORY   {   rom (rx) : ORIGIN = 0x08010000, LENGTH = 1024k - 64k   ram (rwx) : ORIGIN = 0x20000000, LENGTH = 128k   ram1 (rwx) : ORIGIN = 0x10000000...

Robmar by Senior III
  • 2434 Views
  • 7 replies
  • 0 kudos

How to add arm-none-eabi header files for example:(stdlib.h,string.h) in a protected region in linker script section?

I have mentioned few files in protected region and calling function of unprotected region through a different region with the help of pointer, but when I am modifying those functions which are in unprotected region ideally my protected region should ...

TShad.2 by Associate
  • 971 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE won't open

I have just installed the STM32CubeIDE ,but am unable to open it for some reason , am clicking its icon but nothing is happening. Any got any ideas how i can resolve this ?

ACern.1 by Associate
  • 1593 Views
  • 2 replies
  • 0 kudos