STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1431 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 560 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Using gated timer with STM32CubeIDE, HAL, and STM32F103 MCU?

I want to create a simple demo for a gated timer in STM32F103. I am using STM32CubeIDE but I cannot find the right way to configure Cube and use HAL functions to make it work.I have set up TIM1 timer to run at a 1kHz clock in slave mode (gated mode),...

AQuev.1 by Associate II
  • 1284 Views
  • 0 replies
  • 0 kudos

Resolved! STM32F303K8-Nucleo-Example (ADC_DMA_Transfer): undefined reference to `HAL_Init' - BUT include paths are configured

Hi,im trying to get this example to work, but it sont compile. The paths for all includes are set up with a link folder in the project.I double checked those, but cant get to the problem.The order is: "main.c -> main.h -> stm32f3xx_hal.h -> HAL_Statu...

Tobe by Senior III
  • 2839 Views
  • 1 replies
  • 0 kudos

STMCubeIDE USE_HAL_***_REGISTER_CALLBACKS definition

Hi all,I'd like to register some user defined callbacks using the HAL_***_RegisterCallback() functions. I understood that first I need to define the compilation flag USE_HAL_***_REGISTER_CALLBACKS but where should I put it? Looking through the variou...

LLea by Associate
  • 18481 Views
  • 28 replies
  • 14 kudos

No rule to make target `clean' ?

Hello,I use STM32CubeIDE v 1.4.2 It appeared today during the build my project:make clean make: *** No rule to make target `clean'. Stop."make clean" terminated with exit code 2. Build might be incomplete.11:48:08 Build Failed. 1 errors, 0 warnings....

Peko by Associate III
  • 11133 Views
  • 7 replies
  • 1 kudos

Resolved! CMake 3.20 or higher is required

HI I try to import my Stm32cubeIde project into VSCodeI have install STM32CubeCLTthe configuration failed with this error [variant] Loaded new set of variants[kit] Successfully loaded 5 kits from C:\Users\XXXXXX\AppData\Local\CMakeTools\cmake-tools-k...

LHOUE by ST Employee
  • 4434 Views
  • 4 replies
  • 0 kudos