STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1658 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 621 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Timer(32bit) Inputcapture

STM32H745i Discovery kit :In this board TIM2/5 are 16/32 bit  timers when am going to configure in cubeIDE there Prescalar is 16bit  . How can  i use 32bit timer ??  and in this board input pin terminations are very crucial  ?? Any help would be than...

SA  V.1 by Senior
  • 2892 Views
  • 2 replies
  • 0 kudos

STM32 Cube IDE Update Not Working

Hi, I am working on a collaborative project. Someone sent me a new version using an updated version of STM32Cube IDE, and now the .IOC throws an error when I try to open it:To fix this, I try running Help > Check For Updates, but this gives me the fo...

image.png image (1).png Screenshot 2023-08-08 at 5.40.10 PM.png
EPala.2 by Senior
  • 3325 Views
  • 2 replies
  • 1 kudos

NetX client is getting stuck

 Hi, I am facing some strange issue of Suspended NetX client while receiving TCP packet from Server running from Ubuntu PC. I am attaching screenshot where App TCP thread and Main Ip Instance are getting suspended all of a sudden or if I give a break...

Nitin by Associate III
  • 1111 Views
  • 0 replies
  • 1 kudos

run inference of array input and serial port

I'm trying to run inference of Onnx model. I tried to use the manual 'How to run locally a c-model'. in all the guides I found the input for the network is one number in my case the input is array of[1][32][101].I want to inference the array once so ...

audi by Associate II
  • 940 Views
  • 0 replies
  • 0 kudos

Resolved! TSC Groups on L432KC

Hey there,I'm just getting started with touch sensing on the STM32L432KC, therefore I wondered about the following: I can just see "Group 2" in System Core > TSC (See picture). "Group 2" implicates, that there is a "Group 1".Is there also a "Group 1"...

akarger_0-1691575078199.png
akarger by Associate
  • 1759 Views
  • 2 replies
  • 1 kudos

STM32 lwip tcp server error

I was going to make a lwip tcp server that was implemented in cube mx on cubeI get an initialization error, but I can't see it on tube mx, but it worked, so I wanted to ask how I can fix this to get rid of the errorPlease tell me howThe part where th...

ark2 by Associate III
  • 1344 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.