STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1564 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 593 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Debug Error on Dual Core STM34H747I-DISCO Board

Using Application Note AN5361 and a Online ST Video. I have create a project in STM32CubeIDE for the STM32H747I-Disco Board. As a test of the debugging, I have have both cores simply blinking separate LEDs.I set up the CM7 debug configuration  per AN...

SLimi1_0-1691289197359.png
SLimi.1 by Associate III
  • 2643 Views
  • 3 replies
  • 0 kudos

Keil MDK to STMCube IDE project conversion

Hi.Bought the Arm Education Media book "DSP using Arm Cortex-M based Microcontrollers" along with the SMP32F407G-DISC1 board and the LTEK audio board. Got the LTEK audio loop thru example working under Keil.Now trying to get this project working unde...

waddy by Associate II
  • 1720 Views
  • 0 replies
  • 0 kudos

How to operate STM32 power on off

We implemented a lwip tcp server with STM32 and even sent and received messagesBut when I was debugging, it was good I'm trying to disconnect ST-LINK and see if it works by turning the power on and off without debugging, but the server didn't even cr...

ark2 by Associate III
  • 2087 Views
  • 2 replies
  • 0 kudos

Use LWIP in C++ main file

Hi every oneHow can I use LWIP TCP connection(socket, NetConn, Raw ... )  in main.cpp   ?I can use Raw in main.c properly but I need to use it in cpp files. thank you

MTora.1 by Associate III
  • 1072 Views
  • 0 replies
  • 0 kudos

STM32F4 Problem with USART

Hi, I want to use USART2 as transmitter on stm32f429zi mcu (nucleo board). I configure registers as in the picture, but transmission don't work. I use USART2 on PA2 pin and I need transmission with 115200 baudrate, alternate function is AF7 and usart...

[Debug] Software reset with bootloader

Hello everyone,on my MCU i've loaded a bootloader at address 0x0800000 and a dummy application at 0x0810000, but i'm experiencing some issues on chip reset button on the IDE. At first, when i debug the application no errors are encountered and the ap...

PGior.2 by Associate II
  • 2953 Views
  • 4 replies
  • 0 kudos

Resolved! STM32CubeIDE select target device

Hello,I have 2 NUCLEO boards connected to my computer and I don't see any option to select the target device when I run my project in STM32CubeIDE. I want to be able to run a different program on each board, how can I achieve that ?

Colus by Associate
  • 4200 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.