STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1407 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 556 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Installing CMSIS and CMSIS_DSP - missing files

Board H745ZII have installed ARM.CMSIS  5.8.0 and CMSIS-DSP 1.15.0 via the IOC>Software packs> and selected the components I want available under Select components. I have then enabled them under Middleware and software packs so CMSIS and CMSIS-DSP a...

MEde.1 by Associate III
  • 3300 Views
  • 2 replies
  • 0 kudos

read_memory: failed to read memory

 I'm trying to debug with an STM32H753BI using openocd and gdb using cube ide but im getting error like failed to read memory.here is the log:xPack Open On-Chip Debugger 0.12.0+dev-01312-g18281b0c4-dirty (2023-09-04-22:31)Licensed under GNU GPL v2For...

user_gk by Associate
  • 3917 Views
  • 3 replies
  • 0 kudos

STM32L476 Hard Fault during startup

Hello, I realised an stm32l476 board. After receiving the board, we tested all the connection power.. All is good.To start with the coding I added a simple code to toggle pins to check the functionality. The code install successfully on the board. Ho...

NIXAIRSOLUTIONS_0-1700097730756.png NIXAIRSOLUTIONS_1-1700097765714.png

Resolved! Parse HEX File to HAL_FLASH_PROGRAM()

Hello everyone, I want to make bootloader, everything is done, but not working.  1. I create two apps in STM32CubeIDE:BOOTLOADER: 0x08000000APPLICATION: 0x08020000I did simple program and I jump from app to boot, and from boot to app (It's works fine...

Martini by Associate II
  • 5662 Views
  • 7 replies
  • 1 kudos

Resolved! Connect debugger without uploading binary

Hi there,I'm using ST_Link V3 with H743 MCU. For short debug sessions it works seamlesly.For longer run-time I have to disconnect my computer with CubeIDE and go home, but MCU stays running.Next day, I need to reconnect Debugger and check the state o...

DrDro by Associate III
  • 3115 Views
  • 3 replies
  • 1 kudos

uart_ERROR callback triggered but errorCode is zero

I am programming a STM32 nucleo-f746ZG development board where I am using USART2 with RX interrupt.I have setup USART using CubeMx (async, baud:250Khz, data: 8, stopBit: 2, noParity). I am reading a single byte from a DMX stream by calling HAL_UART_R...

Resolved! What OS is running on the stm32 eval board?

Hi,I am using Cube IDE to study. And the boardNucleo-uaa5zj-q.My first program "Hello World" is printed well on the console.But I would like to know what OS is running on this board?If it is Free RTOS, in Pinout & Config -> Middleware, why could I ch...

shiacapt_0-1701219601177.png
shiacapt by Associate
  • 1879 Views
  • 1 replies
  • 0 kudos