STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1554 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 588 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Problem with FreeRtos in TrustZone enabled

Hi Hi We are using product STM32H56 series , I am encountering problem while building my project I am using STM32cubeIDE , trust zone enabled .I enabled X-CUBE-FREERTOS  M33non secureIn software package I installed   -STm X-CUBE-FREERTOS  -CMSIS RTOS...

Kendall7_0-1711444735447.png Kendall7_1-1711444777776.png
Kendall7 by Associate II
  • 2664 Views
  • 3 replies
  • 0 kudos

STM32F401RCT6 EEPROM Emulation

Hi,I need to use EEPROM Emulation for my project's needs. I'm using STM32F401RCT6. I tried to use EEPROM emulation in STM32F40x/STM32F41x microcontrollers (AN3969) but after several tries, I only got errors as screenshot at below:Any help would be ap...

omeraydin_0-1694421990342.png

STM32L476 EEPROM Emulation

I have followed the eeprom emulation described in X-CUBE-EEPROM expansionhttps://www.st.com/en/embedded-software/x-cube-eeprom.htmlBut the solution was written using the old STM32 standard API. Does somebody knows about an EEPROM Emulation solution t...

RLeva.1 by Associate
  • 5005 Views
  • 2 replies
  • 0 kudos

Resolved! Power Regulator Voltage scaling and SysClock issue

Hello,I am using STM32H755 microcontroller and STM32CubeIDE V1.13.0 for my development.I am not able to set the clock frequency to 480MHz. Whenever I do so, I receive power regulator voltage scaling error. (Shared in the attachment).The product revis...

HDesa.1 by Senior
  • 5303 Views
  • 6 replies
  • 3 kudos

IOC project doesn't render completely in CubeIDE

After 100 attempts to open the IOC project inside the CubeIDE it opened but only a half, which makes it unusable, what can I do?CubeIDE/Java is eaten all my CPU, but they aren't doing any useful work, help please! 

Captura de pantalla de 2024-03-25 21-51-51.png
XR.1 by Senior
  • 1129 Views
  • 0 replies
  • 0 kudos

Trustzone: NonSecure_Init does not start the nonsecure

Whilst using the standard code generated through cubemx for Trustzone on the Nulceo-WBA55cg Board with TZEN = 1 and having the nonsecure in the Debug configuration of the secure the code doesnt complete the Nonsecure init in the last Line. I checked ...

Isko by Associate II
  • 1638 Views
  • 1 replies
  • 0 kudos

Convert Integer to float

Hello everyone, can someone tell me why casting doesn't work. I want to convert int values of an array to float.for (int i = 0; i<= adcBufferSize; i++){adc_buffer_float[i] = (float)adc_buffer [i];}

Sax by Associate III
  • 8567 Views
  • 12 replies
  • 2 kudos

Resolved! Include not works in STM32CubeIDE

STM32CubeIDE Version: 1.14.0 Build: 19471_20231121_1200 (UTC) OS: Windows 10, v.10.0, x86_64 / win32 Java vendor: Eclipse Adoptium Java runtime version: 17.0.8.1+1 Java version: 17.0.8.1include setupand the exported xml content<option IS_BUILTIN_EMPT...

sayhi2008_0-1710982545148.png
sayhi2008 by Associate II
  • 2692 Views
  • 3 replies
  • 0 kudos

Resolved! application is stuck at SystemClock_Config() and MX_RTC_Init().

 Hi,I have debugged my application and came to know, there is problem at SystemClock_Config(); yet I do not know what the issue, please see clock configuration in below as well.I have also commented out SystemClock_Config() and debugged again, this t...

demir_0-1711204698179.png
demir by Senior II
  • 3042 Views
  • 1 replies
  • 0 kudos

Resolved! UART is not working

Hi,I have checked connections and assured that everything is set up correctly. When I run the below code, I cant see anything on serial console.Does anyone have any idea about the root cause ? /* USER CODE BEGIN Header */ /** **********************...

demir by Senior II
  • 7120 Views
  • 18 replies
  • 7 kudos