STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1550 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 588 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

what is ~/STM32Cube/Repository

During seeking for space on my macOS hard drive I found 12GB of files in~/STM32Cube/RepositoryWhere do they stem from? Can I delete them? Has it got to do sth. wit STM32CubeIDE? 

Resolved! I2C Not Working

Hello,I am trying to setup an external ADC/DAC module with an STM32H7 microcontroller. I2C Slave - EVAL-AD5593R-PMDZI2C Master - STM32H757XIH6 on STM32 Embedded Display by RiverdiI am struggling to get the very basics of communication to work as I ca...

Resolved! STM32 Cube IDE 1.15 USB Middleware Codegen Bug

Steps to reproduce:Create a new project with an STM32F779NIH processorEnable USB OTG highspeed (device only)Add USB_Device middleware (select any class)Generate the project codeInside the USB_DEVICE/App/usbd_desc.c file, the GetSerialNum(void) functi...

DrWidget by Associate II
  • 4402 Views
  • 6 replies
  • 4 kudos

can't open project if folder is already imported

I'm trying to open the example project "GPIO_InfiniteLedToggling". Apparently I did tis nce because I can't choose the project since "folder is already imported as project". If I choose (what I assume to be the created project) "GPIO_InfiniteLedToggl...

Jamiw by Associate II
  • 5222 Views
  • 5 replies
  • 0 kudos

Resolved! How to confirm firmware

I’m using STM32CubeIDE headless-build script in Linux for developing the software.I have a question regarding how to check the version of the firmware that I’m actually using in my environment.I tried to set a certain version of the firmware by writi...

u1kano by Associate III
  • 5140 Views
  • 7 replies
  • 0 kudos

Help need with ST-LINK_gdbserver.exe

When trying to debug debug or run I got: terminate called after throwing an instance of 'std::logic_error'what(): basic_string::_M_construct null not valid I tried to run this manually and I got the same:C:\ST\STM32CubeIDE_1.15.0\STM32CubeIDE\plugins...

dhs by Senior
  • 1064 Views
  • 0 replies
  • 0 kudos

Resolved! STM32Cube IDE STM32F4 Discovery board I2S DMA

Hi AllTrying to get an understanding of how I2S with DMA works using the STM32Cube IDE by implementing a simple audio loop-through application.Connected the STM32F407G Discovery board to a Digilent PMOD I2S2 codec and set up using the STMCube IDE GUI...

waddy by Associate II
  • 7291 Views
  • 7 replies
  • 2 kudos

Resolved! STM32CubeIDE Serial Port Connection

I  have a STM32F405 and am trying to setup UART to connect to my pc. As of now I have connected it with an ST-Link/V2 and later on want to program it over USB-C using UART. See the wiring diagram:I have used PA10 and PA9 for RX and TX.The parameter s...

mathieusteketee_3-1713883700752.png mathieusteketee_4-1713883730791.png mathieusteketee_5-1713883780385.png mathieusteketee_6-1713884880999.png