STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1549 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 588 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

SVW console - no output after few seconds

I am using SWV ITM console (printf output) and SWV Data Trace Timeline Graph. They works only few seconds and then no output, while the program still works (LEDs reacts on interrupts, etc.) only no SWV debug outputs are provided.I am using STM32G474R...

ondra by Associate
  • 1833 Views
  • 2 replies
  • 0 kudos

Fault analyzer toolbar missing

Hello everybody,Since I did last update of STM32CubeIDE software I cannot see the fault analyzer toolbar anymore (attached file img).Am I missing some configuration to display it?Or is due to the update?Thank you for your time 

lucius92 by Associate
  • 4314 Views
  • 5 replies
  • 0 kudos

B-U585-IOT02A BSP example issues

Hello forumI have just purchased the B-U585-IOT02A and would like to start and interact with all of the sensors on in,for it, I tried the IDE example of the BSP in general, but it didn't even compile. even after trying to manually use the driver noth...

Resolved! CubeIDE linked list code generation error

Hi all,I'm using STM32Cube IDE (version 1.15.1 Build: 21094_20240412_1041 (UTC)) and have the STM32H573 chip with the LinkedList feature.Unfortunately the code generation of the linked list does not work properly and forgets to set some config settin...

joker_0-1716281151165.png
joker by Associate
  • 1650 Views
  • 1 replies
  • 1 kudos

Resolved! Defined symbol no take value

Hi i have defined a Defined symbol "COST=3" in setting compiler like thisstm32cube color fine the code but during execution it is like if COST=0you can watch the execution cursor are on the #else (and numBB are = 0) How can i fix it? 

bug stm32 1.png bug stm32 2.png
sifour by Associate
  • 1725 Views
  • 2 replies
  • 0 kudos

Resolved! IDE generated elf file, unexpected behavior

Hi there,I developed a custom bootloader for a STM32H755 MCU.I successfully tested my bootloader on a NUCLEO H755  board (with small projects), and all seems ok.Moving on my final board, with the actual Firmware to be downloaded I'm experiencing an u...

iTTy_0-1715694543737.png
iTTy by Senior
  • 2066 Views
  • 2 replies
  • 2 kudos

Resolved! USBPD for STM32L562

Hi ,      I was given by a task to connect an external load to STM32L562 for USBPD. Do you guys have any idea how to start and what to do in the inital process. Task details Support all 100W+ USB PD EPR power profiles using standard USB PD 3.1 parame...

nishadh by Associate
  • 1498 Views
  • 1 replies
  • 0 kudos