cancel
Showing results for 
Search instead for 
Did you mean: 

USBPD for STM32L562

nishadh
Associate

Hi ,

      I was given by a task to connect an external load to STM32L562 for USBPD. Do you guys have any idea how to start and what to do in the inital process.

 

Task details 

Support all 100W+ USB PD EPR power profiles using standard USB PD 3.1 parameters, 100W (20V @ 5A),  140W (28V @ 5A) , 180W (36V @ 5A) , 240W (48V @ 5A).  240W may not be able to be tested during this phase due to market availably of OTS 240W supplies, however functionality should be added for future use
Requires an external load on the module connectors to validate power delivery output capability

 

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
FBL
ST Employee

Hi @nishadh 

TCPP upgrade to support EPR voltages is ongoing ;)

For further details, check this thread Solved: Re: USB PD sink - STMicroelectronics Community

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL

View solution in original post

1 REPLY 1
FBL
ST Employee

Hi @nishadh 

TCPP upgrade to support EPR voltages is ongoing ;)

For further details, check this thread Solved: Re: USB PD sink - STMicroelectronics Community

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL