cancel
Showing results for 
Search instead for 
Did you mean: 

Why cannot use the open project menu?

JohnsonWang
Associate

When I run STM32CubeIDE, the open project menu is disabled (in grey color). How can I active it?issue.jpg

1 ACCEPTED SOLUTION

Accepted Solutions
Karl Yamashita
Principal

You need to highlight the unopened project in the project tree. Then you'll be able to open the project. If you want to work with an existing project that isn't in your project tree, then you need to import the project.

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.
CAN Jammer an open source CAN bus hacking tool
CANableV3 Open Source

View solution in original post

2 REPLIES 2
Karl Yamashita
Principal

You need to highlight the unopened project in the project tree. Then you'll be able to open the project. If you want to work with an existing project that isn't in your project tree, then you need to import the project.

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.
CAN Jammer an open source CAN bus hacking tool
CANableV3 Open Source

JohnsonWang
Associate

Thank you so much! The issue has been fixed.