User Activity

I have set up a UART as receiver. I use circular buffer to copy the data in. The code pretty much works ok with one exception:If the last byte of incoming data frame is to be saved in index 0 (UARTRx[0]), the data appears at this address AFTER the bu...
Im creating an RTOS queue in the configuration tool. Whowever if I try to place anything in the queue the program crashes.Configuration: Generated Initialization Place item in queue (btn.dec is a uint8_t variable) Debug As you can see the item size i...
I want to hide the colored progress bar in circleprogress widget when there is no data. I can hide the whole widget but how can I keep the background image(a grey circle) in place. If i set the value to 0 there is still a small dot that remains. I as...
Does anybody have an idea why the settings button is grayed out?MCU: STM32F412Other settings seem fine to me: 
Using TouchGFX Designer 4.22.0Why it is not possible to make a circle progress much like a car dashboard would have. Zero is at about 7 o'clock and full is at 4 o'clock.The circle progress always starts at 12:00. No mater what parameters I enter.Is t...