cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE 1.18 Freezes when trying to import project from 1.16

Carl_G
Senior III

I had the latest version of 1.16 installed. I upgraded that installation to 1.18 which was just released. When I double click the ioc file it asks if I want to continue or to migrate. When I choose migrate it doesn't work. It freezes and I have to close the IDE and restart it. After fighting with this for a day, I downloaded 1.18 and installed it in a separate directory. This installation had no problem migrating. I attached the eclipse log file.

 

Carl_G_0-1742176015691.png

 

2 REPLIES 2
Semer CHERNI
ST Employee

Hello @Carl_G 

First let me thank you for posting.

Could you share the ioc file.

KR,
Semer.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Carl_G
Senior III

IOC file attached