STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

STM32WL5MOC Delevopment Issues

Hello everyone,   I'm trying to setup a STL32CubeIDE project with a custom STM32WL5MOCH6 MCU. I managed to test if the board is alive with a simple hello world debug print on SWV and there's no issues.   The problem starts when I enable the LORAWAN m...

yaxsomo_0-1743808292364.png yaxsomo_1-1743808352997.png yaxsomo_2-1743808375160.png yaxsomo_3-1743808396473.png
yaxsomo by Associate III
  • 2610 Views
  • 6 replies
  • 1 kudos

Resolved! STM32WBA55CG ADC DMA CIRCULAR

hello,I want to set up a timer2 TGO triggered DMA system with 60 samples in 20ms from 4 channels.I made the linked_lisit settings etc. via CubeMx but I can't get a sample from the ADC.Can you help me?

Resolved! aci_gap_adv_set_scan_resp_data returns 0x0C

Hi allwhen i try to call the function to add scan response data to my advertising data I get the error 0x0C. I get the error code means that operation is not allowed, but nowhere it tells how to call a function in order to be allowed. I am susing STM...

cvs_dev_0-1747230228710.png
cvs_dev by Associate II
  • 1113 Views
  • 1 replies
  • 0 kudos

Resolved! How to obtain the .ioc file

在 STM32Cube_FW_WB_V1.22.1\Projects\P-NUCLEO-WB55 下。Nucleo\Applications\BLE 中,某些文件有。IOC 文件,而其他文件则没有。例如,在 BLE_CableReplacement 中,没有。与 STM32CUBEMX 相关的 IOC 配置文件。如何获得?

Thorn by Associate
  • 1963 Views
  • 4 replies
  • 1 kudos