STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 221 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4067 Views
  • 0 replies
  • 3 kudos

X-NUCLEO-WB05KN1 - Zephyr Problem

Hi, I have attached a X-NUCLEO-WB05KN1 on top of a NUCLEO-H743ZI2 board and are trying to verify whether it works by flashing the peripheral_hr sample with the shield argument "x_nucleo_wb05kn1_spi". Sadly it does not work (it is stuck in bt_spi_open...

CBras by Associate II
  • 2037 Views
  • 4 replies
  • 2 kudos

Resolved! Trouble achieving low current in STOP2 mode on STM32WB55CGU6

Hi everyone,I'm facing a frustrating issue and would really appreciate any help or insight you could provide.I’m trying to get the STM32WB55CGU6 into STOP2 mode, but I consistently see current consumption over 600 µA, both on my custom PCB and on the...

ppk-20250508T144338.png
r3v1 by Associate II
  • 2701 Views
  • 7 replies
  • 1 kudos

STM32WB OTA Reboot Failing

Hi there,I'm developing a custom application for FUOTA (Firmware Update Over The Air), targeting an STM32WB55-Nucleo devboard. I’m referencing AN5247 and AN5289 and using the BLE_OTA example from STM (open source code in new page). My user applicatio...

step_stuck.png image.png image (1).png custom_app_no_response.png
bspfino by Associate
  • 2166 Views
  • 3 replies
  • 0 kudos

LSE failure Detection Problem

Hi,I am using STM32WBA52CGU6 controller.I configure Pins of LSE_IN and LSE_OUT.Without generating frequency at this LSE_IN Pin I got detection as LSE is on but actually LSE_IN is just open.I attached System clock Config code below:-/** Initializes th...

Resolved! Documentation for STM32WL5Moc

Hello, Where can I find information, such as flash memory layout, RAM addressing, peripherals configuration for the SMT32WL5MOC ? The product page has quite a few documents, but nothing that is really usefull for developing firmware....