User Activity

Hi,I am trying to write a battery powered application with a STM32WL5MOC. The LoRa capability and the form factor are crucial. The dual-core feature unfortunately makes everything so much more complex. I only need the CM0+... so in the future the CM4...
Hi everyone,I have an odd behaviour here. I got a STM32L496 with FreeRTOS on it. The CPU is very busy (15 task running, flash size is almost 1MB). I am using the latest STM32CubeIDE 1.14.1.Now I'd like to remove something from a std::vector, so I do ...
Hi,I recently upgraded to macOs14.2 while running IDE@1.13.2. This worked for a while... 2-3h. All the sudden the IDE kept crashing on me. So I upgraded to 1.14.0 which did not solve the problem. I can't even press on the small > icons to drop down a...
Kudos given to