NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
It's quite annoying that the names of the BLE stack are cut off, even though there's plenty of free space. The browser doesn't matter. My screen resolution is 2496 x 1664, with 150% scaling on Windows.
Hello everyone,I was trying to build communication between 2 LoRa devices. Sending a "Hello" from Tx board and receiving on Rx board. I tried to debug using UART (printf through Tera Term). But I am stuck at transmitting data. Do any of you have an i...
Hello,I'm having problems with the FUS not starting and the Wireless stack not responding.In my code, the wireless stack can be updated. In the process of updating it, the STM32WB55 was interrupted by an external reset, and the FUS was left unrespons...
After performing an OTA update, the Bluetooth icon appears as shown in Figure 1, but it does not display the "STM_OTA" name.The correct result should look like Figure 2.I followed the modification steps from this video, including adding the OTA Rebo...
Dear Team, May I know STM32WBA52CG support some basic AI/ML applications. We don't need controllers like STM32N6. If STM32WBA52CG supports some basic AI/ML can you please share some materials,applications notes or some examples where I can see some A...
After I select the project and download it, the ST BLE Toolbox (as shown in Figure 1) displays "Upload completed."However, after the Bluetooth restarts, it still shows "STM OTA", which means my application was not successfully downloaded to flash.I'm...
Hello,I built two PCBs, one with the STM32WL33KCV6TR (QFN32 version) and one with the STM32WL33CCV6TR (QFN48) version. Both schematics are identical (48MHz + 32768Hz crystal connected, SMPS used, decoupling capacitors on power pads, otherwise nothing...
Hi STTwo-32, I have 2 more questions: 1. What jumper to remove - so the NUCLEO board will stop advertising ? 2. What to do - to change power on STM32WB5MMG module from current 2.4-2.6V to 3.3V ? Thanks
Why there is no NUCLEO-WBA52CG projects in STM32CubeWBA?What caution should be taken when using STM32WBA52 in STM32CubeWBA?
Having checked the ST Website for LoRaWAN kits I settled on the LoRa LF Sensor and Gateway kit (P-NUCLEO-LRWAN3) There is no mention on the website that this pack is obsolete or end of life. I always check that because I have been burned before by ST...