2024-12-17 4:42 AM
I am currently working with the STM32WB55RGV6 MCU and utilizing the BLE functionality provided in the BLE_p2pserver example (STM32Cube_FW_WB_V1.18.0) from ST. However, I am facing a limitation where the data packet size is restricted to 20 bytes, preventing me from sending larger amounts of data.
I have come across forums suggesting that the MTU size can be increased to enable higher data throughput. However, I am not very experienced in writing or modifying the software, and I need step-by-step guidance to implement this change correctly.
I also found Application Note AN5289 and investigated the section on "How to maximize data throughput". While the document provides suggestions, I am unsure how to apply them to my code.
Could you please provide clear, step-by-step instructions on how to:
Your help would be greatly appreciated, as I am currently stuck on this issue.
Thank you!
2024-12-18 5:57 AM
Hello @EBard.1
1) You can increase the MTU size throw the #define CFG_BLE_MAX_ATT_MTU on the app_conf.h file.
2+3) to understand how those recommendations work, you can take a look at the BLE_DataThroughput.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-12-19 11:41 PM - edited 2024-12-19 11:45 PM
Hi,
Thank you,
Currently I am using BLE_p2p example provided by ST. 
I found that forum, should I go over these suggestions? Is there anything to add on these suggestions? 
https://community.st.com/t5/stm32-mcus-wireless/aci-gatt-update-char-value-ext-issue/td-p/652328
Should I add these?:
* hci_le_set_data_length
* hci_le_set_phy
Can you guide me like on the link please? Thank you. 
2024-12-19 11:56 PM
Hello @EBard.1
I think that following the recommendations of my answer on the last post should do the job.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-12-20 12:05 AM
Hi,
Should I add these functions, what do you think?
* hci_le_set_data_length
* hci_le_set_phy
Thank you for your answers!
2024-12-20 12:12 AM
I don't think so. But you could try.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-12-20 1:24 AM
Thank you again, for that function:
aci_gatt_update_char_value_ext(0x0000, aPeerToPeerContext.PeerToPeerSvcHdle, aPeerToPeerContext.P2PNotifyServerToClientCharHdle, 0x00, 509, 0, 243, (uint8_t *) pPayload);
Should I use 0x0000 adress for the Update_Type ?
2024-12-20 1:45 AM
This parameter depends on the client(s) you want to select to be notified.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.