STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 221 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4067 Views
  • 0 replies
  • 3 kudos

STM32WL reset in debugger mode

Hello All,I am working on STM32WLE5 , and low power mode used for controller is stop 2 mode. And I am using MSI at 4Mhz  as system clock. When i enable debugger mode, controller takes reset after a while and reset type shown is also not correct. Whil...

Resolved! STM32WB55 Error on start of BLE stack

Hi,I'm currently trying to get Bluetooth working from Zephyr. I'm working with the Zephyr sample codezephyr\samples\bluetooth\peripheral_dis.I'm using a Nucleo-WB55RG board. Using STMCubeProgrammer I've loaded the FUS at 0x080EE000 and the file stm32...

Lee_T by Associate II
  • 3185 Views
  • 11 replies
  • 1 kudos

I-CUBE-LRWAN support for STM32U5 + SX1262

I was wondering if anyone had managed to get the LoRaWAN End-Node example running on other MCUs than the STM32L series. I've been trying to get it to run on the STM32U5A9 combined with an SX1262, but I haven't had any luck. I'm trying to integrate th...

JSGraaf by Associate III
  • 1239 Views
  • 2 replies
  • 0 kudos

difference between MCUs firmware

Hello,      I would like to know if fw developed in stm32cubeIDE for nucleo wl55jc1(there are some examples for it) is compatible with https://www.st.com/en/microcontrollers-microprocessors/stm32wle5cc.html mcu family(stm32wle5ccu6) or I should expec...

Matching networks

HiIm a bit new and have som RF related question.I am doing a heart monitoring project where i want to measure ECG signals, put it through my AFE (analog frontend), then into the ADC inside the MCU and then output the data through BLE into a phone. I ...

siyar by Associate II
  • 810 Views
  • 1 replies
  • 0 kudos

Resolved! cant program FUS and stack.

Hi.I'm working with the EVAL STM32WB5MM-DK for a while now, already programmed the stack and the FUS many times, and it's the first time I got this error.After successfully open STM32CubeProgrammer (v2.19) and connected to the programmer, Selecting t...

netanelu_0-1750019098157.png netanelu_1-1750019210318.png
netanelu by Associate III
  • 999 Views
  • 2 replies
  • 0 kudos

Resolved! Unable to turn on BLE WAPN on extended-full stack

Hey there,i have a custom board designed which is broadcasting stuff over BLE.So far i am using the full_stack_fw which works quite well.In order to turn on extended advertising i wanted to switch over to the full_extended_stack (needed for extended ...

Exeu_0-1750413452410.png Exeu_1-1750413528054.png
Exeu by Associate III
  • 1378 Views
  • 4 replies
  • 1 kudos

pROBLEM WITH stm32WB05KZ wake-up proccess

Hi, I'm having a problem with the wake-up procces using interruptions. I use three pins, PA0, PA8 and PA9, set the with no pull-up, and in rising mode. then i enable them as wake up pins, in rising mode. i go to sleep in stop mode, using the function...

LuisL by Associate
  • 729 Views
  • 1 replies
  • 0 kudos