Hi,I have several questions regarding current consumption numbers as they appear in the Datasheet of the STM32WLE5.in Table 28 / Table 29 the current consumption of LORA RX/TX modes is mentioned.I have several questions:1. is it possible to use a TCX...
Hi,Does ST provide the S-Parameters model for the RF pins of the STM32WLE5 device in order to use it in AWR Micro wave office simulation of the RF chain of a board ? Thanks,Viola
Hi ,you mentioned I need to add 1.5mA due to the TCXO consumption.1. Do you assume that the external TCXO requires 1.5mA and thats the reason you mention 1.5mA ?or , 1.5mA is the additional current required by the STM32 VDD and its in additio...
Hi ,I already saw this application note.I was wandering if we can do a complete simulation of the RF path -using the S-Parameters model of RF pins of the STM32wle5 since we want to investigate for example added filters performance on different freque...