STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 221 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4067 Views
  • 0 replies
  • 3 kudos

STM32Wl5M Flashing issue

Hello,I'm trying to flash the example program in B-WL5M-SUBG1 connectivity expansion board, and below issue.Tried with different EVK boards but still the persists.I got a popup for updating firmware of STLINK-V3MINIE debugger, so I upgraded the firmw...

PrakashN_0-1748143072073.png PrakashN_1-1748143185856.png
PrakashN by Associate
  • 782 Views
  • 1 replies
  • 0 kudos

Stm32Wl55jc cannot recieve downlink in Class C

Hey, I am new to lorawan. I am using AWS iot core as my LNS. I am able to recieve downlink in class A after an uplink. But when I try to recieve downlink in class C mode I am unable to even class C works as class A where the downlink is recieved afte...

SorabhR by Associate
  • 732 Views
  • 1 replies
  • 0 kudos

STM32WLE5CCU6 LoRa Antenna design review

Hi,I want to design my own LoRa-Board based on an STM32WLE-Chip. It is my first time handling with RF-related topics which is why I'm creating this post. I created a design which I would want to have reviewed for major flaws, so I can order my first ...

Resolved! Programmed STM32WLE5CC

Greetings,To start with stm32 wireless series i bought STM32WLE5CC and uploaded my custom code of gpio toggeling without initialiazing PA13 and PA14 for serial wire debug. The program runs as it should but when i try to re-flash the controller with S...

B-WB1M-WPAN1

Colleagues,I need to implement the BLE_CableReplacement project on the b_wb1m_wpan1 device. Since I don’t know the services of this project (the BLE_CableReplacement.ioc file is not included), I tried to adapt the project for the b_wb1m_wpan1 device ...

STM32WBDK LPM wont allow PWM to work

 I’m driving a hobby servo on the STM32WB5MM-DK Discovery board using TIM2 PWM and the STM32CubeWB Sequencer/LPM utilities. When I disable low-power mode entirely, the servo moves flawlessly on each 500 ms button-hold toggle. But as soon as I allow t...

Resolved! Nucleo-wl55jc - LDO / SMPS

Hello everyone,I'm using Nucleo-wl55JC boards with the PingPong example code (which is working). I saw in the datasheet that we could have 2 different power supplies LDO and SMPS, I also saw that the SMPS mode was more economical than LDO, that's why...

KYZ by Associate III
  • 1097 Views
  • 2 replies
  • 0 kudos