STM32WLE5 clock section tab in the Cube-Mx
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2024-11-11 7:22 PM
Hi ,
Regarding working with the STM32WLE5 with SUBGHZ block in the CUBE-MX.
in the clock section tab in the CUBE-MX I dont see any mention of the RF-PLL clock.
if i understood correctly - in order to work with the LORA SUB-GHZ BLOCK i need to supply a 32 Mhz HSE clock .
I dont see in the clock section tab in the CUBE-MX any mention of this "must -have" 32 mhz HSE clock .
it seems any clock source is possible and any frequency is possible .
Does the clock section tab in the CUBE-MX dont represent the CLOCK tree in the STM32WLE5 ?
I see this issue even when I open example code for sughz block within the CUBE-MX.
Thank you,
Viola
Solved! Go to Solution.
- Labels:
-
STM32WL series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2024-11-22 10:23 AM
Hello @viola
There are 2 'main' clocks for 2 independent system:
- Radio always sourced from HSE TCXO.
- The sys clock for the system and Cortex and IPs. This is by default on MSI. Can also be sourced from the HSE (e.g. TCXO), HSI.
I've request to add a warning or a restriction on using the Radio module without HSE enabled (internal ticket number 196877).
The RF-PLL is used as the frequency synthesizer for the generation of the local oscillator
frequency (flo) for both transmit and receive chains. The RF-PLL uses auto calibration and
uses the 32 MHz HSE32 reference. So, it is not a Clock that should be set on the clock tree of the MX, it works will HSE is available, and it can be set by Set_RfFrequency() command that take the Channel RF frequency as input (868MHz...).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2024-11-22 10:23 AM
Hello @viola
There are 2 'main' clocks for 2 independent system:
- Radio always sourced from HSE TCXO.
- The sys clock for the system and Cortex and IPs. This is by default on MSI. Can also be sourced from the HSE (e.g. TCXO), HSI.
I've request to add a warning or a restriction on using the Radio module without HSE enabled (internal ticket number 196877).
The RF-PLL is used as the frequency synthesizer for the generation of the local oscillator
frequency (flo) for both transmit and receive chains. The RF-PLL uses auto calibration and
uses the 32 MHz HSE32 reference. So, it is not a Clock that should be set on the clock tree of the MX, it works will HSE is available, and it can be set by Set_RfFrequency() command that take the Channel RF frequency as input (868MHz...).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2024-12-18 5:47 AM
Kudos to you - I hope this gets into Cube, as I just ran into this ambiguity myself. Surprising that the clock tree from the datasheet and Cube look so different, with Cube completely omitting the RF line showing the source.
Thankfully I still popped an HSE pad on the design, so I can, hopefully, at least get some dev going on the prototype.