STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 235 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4077 Views
  • 0 replies
  • 3 kudos

Resolved! direct advertising stm32wb

i cant seem to really connect to my iphone after direct advertising i get a false print that i have connected Bonded device 0 / 1 - Public BLE address xx:xx:xx:xx:xx:xx -- here it prints my true iphone bluetooth mac addraci_gap_add_devices_to_list() ...

yam by Associate
  • 620 Views
  • 1 replies
  • 0 kudos

Resolved! STM32WB15x - LSE get stuck at startup

Hi,We're faced to a problem when dealing with LSE clock to handle RTC backup using a supercapa connected to the VBAT pin. The LSE configuration under STM32CubeIDE:  The Clock Configuration function:void SystemClock_Config(void) { RCC_OscInitTypeDef...

freecoder_0-1752497125995.png freecoder_1-1752497197333.png freecoder_2-1752497788124.png

Resolved! How to build DEBUG in BLE_Ota app?

Hi,what i need to do, if i want to build the Debug app of BLE_Ota Demo application (FW 1.23.0)If i import the BLE_Ota app there is only "Release".If i now click on Debug as STM32 Application, the fw is uploaded but then in the Breakpoint i just get t...

Exeu_0-1752569244551.png
Exeu by Associate III
  • 733 Views
  • 3 replies
  • 0 kudos

Resolved! NUCLEO WBA52CG No device found on target

Hello ,I'm trying to flash in the NUCLEO WBA52CG the basic code example available in STM32CubeIDE. I use version 1.19 with Windows. It was originally version 1.17 and was updated in 1.19.No issue to generate the code or build it. I then connected the...

Serge1_1-1752319133876.png Serge1_2-1752319184153.png
Serge1 by Associate II
  • 771 Views
  • 3 replies
  • 0 kudos