STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 226 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4068 Views
  • 0 replies
  • 3 kudos

Resolved! STM32WB5MMG6 BLE_LLD works at 3.3V but not at 1.8V

I'm currently testing the BLE_LLD examples provided by st. I have two Nucleo Boards one running BLE_LLD_Lowpower and one running the BLE_LLD_Pressbutton example. That example works fine and I can change whatever is transmitted.If I use the same BLE_L...

jpepv by Associate II
  • 1854 Views
  • 3 replies
  • 0 kudos

Resolved! Nucleo-WBA65RI FreeRTOS

Hello,I've been doing some test on the NUCLEO-WBA65RI which has a STM32F7 MCU and when I tried to generate a project on CubeMX I noticed that the native FREERTOS option on middlewares does not appear.I see that it can be downloaded using the option X...

RPC by Associate III
  • 777 Views
  • 2 replies
  • 2 kudos

Resolved! Connect two STM32WB MCUs via BLE

Hello everyone,I’m working on a BLE project using two STM32WB55 boards.My goal is to create a connection between them without using the ST BLE Toolbox App.One board is configured as a Custom Server (Peripheral), and the other as a P2P Client (Central...

Resolved! X-Cube-Matter cannot be compiled with MDK Arm

I am developing using X-Cube-Matter v1.4.0.I imported the BLE_Ota project onto MDK Arm and built it, but the following error occurred and I was unable to compile it.../Core/Src/app_entry.c(28): warning: In file included from...../STM32_WPAN/app\app_t...

Resolved! direct advertising stm32wb

i cant seem to really connect to my iphone after direct advertising i get a false print that i have connected Bonded device 0 / 1 - Public BLE address xx:xx:xx:xx:xx:xx -- here it prints my true iphone bluetooth mac addraci_gap_add_devices_to_list() ...

yam by Associate
  • 613 Views
  • 1 replies
  • 0 kudos