NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hi,I'm having a problem with the LSE/RTC and I'm not exactly sure where to start, but I'll try to explain it.I'm using the STM32WB55 and the RTC is used for FreeRTOS tick timing. It works perfectly during normal operation with a 1 ms tick, and it als...
Hi, I try to create a GATT server with a NUCLEO-WB15CC.I'm a beginner with STM32WB MCUs so I followed the Getting Started Series video and particulary : "STM32WB Getting Started Series: Part 12b, Lab. Receiving data from the phone" When its came time...
Basically, my requirement is to run RTC to monitor actual date and time for various schedules to actuate the devices. Note that RTC configuration is provided via LoRaWAN downlink and timestamp after LoRaWAN join.Hence, I would need mix mode to run bo...
I'm using a STM32WL33 on 2 separate custom PCBs. I have one of them being a transmitter only, and I have verified that the transmitter consistently transmits when the keyfob button(s) are pressed (using one of the examples on a Nucleo CC2 board to v...
I'm trying to develop an application for zigbee for the stm32wb55, but i get some problems when I try to reconnect.The configuration for the coordinator its the next parameters: - config.startupControl = ZbStartTypeForm; - config.extendedPa...
Hello guys,I'm new in LoRaWAN so if my question is dumb - sorry guys. Context:Initial info:custom board with STM32WLE5CCUX family MCU on it;LoRa gateway from P-NUCLEO-LRWAN3 pack;private network gateway;activation type OTAA;What is done:gateway from ...
In the STM32WL55 reference manual (RM0453 Rev 1) section 5.8.5 states "Get_Status(status) can be issued at any time"However, there seem to be many situations where this command will result in a reserved value for the "CmdStatus" field.A minimal repro...
I'm currently testing the BLE_LLD examples provided by st. I have two Nucleo Boards one running BLE_LLD_Lowpower and one running the BLE_LLD_Pressbutton example. That example works fine and I can change whatever is transmitted.If I use the same BLE_L...
Hi,I'm currently using a custom board containing a WB55 chipset. My application running on this uses the Thread (open thread) FTD firmware (v1.23.0.0) My understanding is that given a fixed mesh local prefix calls to otThreadGetMeshLocalEid should re...
Hello ST Community,I’m working with an STM32WB55RG NUCLEO board and following the P2P Client tutorial. I’ve encountered an issue where my smartphone(ST BLE Sensor app) is not able to discover the board1. Hardware & Project• Board: NUCLEO‑WB55RG• Exam...