STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 219 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

Low-power mode STM32WLE5

We are developing with the STM32WLE5JC6, everything works, but now we are trying to reduce current consumption. When using the "End node skeleton", it seems to work, however, we are trying to define our own skeleton, because we neither want the ADC n...

STM32WL33CC enters DeepStop but does not wake up

Hello everyone,I'm working on a project using the STM32WL33CC1, based on the example provided in the official ST GitHub repository:https://github.com/STMicroelectronics/STM32CubeWL3https://github.com/STMicroelectronics/STM32CubeWL3/tree/main/Projects...

SergioSI by Associate II
  • 1144 Views
  • 2 replies
  • 0 kudos

lora tx problem using hal lib

I am working on stm32wl5moc controller and lora tx is not working every  time radio status i am getting back is 5 instead of 6, below is the code snipet, and also check the full code attached with this post if (HAL_SUBGHZ_ExecGetCmd(&hsubghz, RADIO_G...

Resolved! LoRaWAN cubemx generated code is showing error

../Middlewares/Third_Party/LoRaWAN/Mac/LoRaMac.c:1650:40: error: 'McpsIndication_t' {aka 'struct sMcpsIndication'} has no member named 'ResponseTimeout'1650 | ( MacCtx.McpsIndication.ResponseTimeout > 0 ) )| ^ The above error is occuring every time ,...

Resolved! lora p2p

"Can someone please check this code? It's for normal LoRa point-to-point (P2P) communication. I’ve attached the file with this post. The problem I'm facing is that a software interrupt is supposed to occur every second and trigger my scheduled task —...

L072Z LRWAN1: Switch from Class C to A

Originally a reply in this old thread: https://community.st.com/t5/stm32-mcus-wireless/not-able-to-disable-receiving-window-of-l072z-lrwan1/m-p/657145@Andrew Neil Sorry for Newbie question, so let's say I want to keep the rx window(in class C) open f...

pho3nix by Associate III
  • 1301 Views
  • 2 replies
  • 0 kudos

Resolved! Lorawan class change

Hello,In our end-node application, the device occasionally needs to switch its operating class from Class A to Class C. This class switching is triggered by an external interrupt rather than a downlink message from the server.To achieve this, I am us...

pho3nix by Associate III
  • 1332 Views
  • 2 replies
  • 0 kudos